Other Parts Discussed in Thread: CONTROLSUITE
Hi, i'm working with the controlStick f28069, I need to use the controlStick in stand-alone without connecting it to an usb port, and powering it by adding 5v at the pin 16.
In order to do this I must shortcircuit the R15, and remove the resistor R9 so the controlStick will boot from flash.
My question is: if I remove de R9 and shortcircuit R15, would I be able to debug with CCS thru the USB port? If the answer is yes, what was the point of adding the R9 resistor?
Thanks
Rodrigo Lebrón