Has anyone been able to get the Spectrum Digital XDS510PP Plus emulator to work with the Concerto controlCARD? I have connected the JTAG to the 14-pin header, and solder-bridged the 7 resistor locations on the controlCARD. I still get the following error:
IcePick_C_0: Error connecting to the target: Error 0x80000244/-2131 Fatal Error during: Register, Initialization, OCS, Cannot access register at 0x00000030
I changed the target configuration file to select the XDS510 Parallel Port-PCI Emulator and chose the correct device.
Is there anything else I need to do? I am using CCS v5.2.0.0069 and have a Release 1.0 of the controlCARD.