Problem No.1
Warnings contents are under the characters:
Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 5.2.3 [C2000]. Another version of the compiler will be used during build: 6.0.2. Please install the compiler of the required version, or migrate the project to one of the available compiler versions. Lab5 properties TI Problem Marker
請協助我解決此問題,謝謝。(本人使用 version is CCV5)
Problem No.2
Please help me. Thanks you.