Sir
In my PCB( solar inverter) ,i have a pin which is pulled down thru 2.2k resistor ,as such this pin is clean wrt the ground of PCB.
But the moment i connect this pin to the ENABLE pin of buffer IC(74hct540),it picks up the switching noise(other input pins of buffer are receiving PWM signals from DSP) whose magnitude increases with the DC link voltage .
The same thing happens if i connect this to a GPIO pin of DSP(TMS320F2812).Actually i need to connect above pin to both of them.(for protection purpose)
The noise occurs during the rise time of PWM signals
I don't think there is anything wrong with PCB as it was made by an expert(still iam not ruling it out......)
I can provide u with schematic of my board if needed.....
plz reply
thanking u
Viju Nair.R