Other Parts Discussed in Thread: DRV8312
I have a customer that would like to do the following to satisfy a test requirement...
- Apply 28VDC Phase A wrt Phase B to hold motor at that pole. Wait ~1 second, then read the motor position via resolver.
- Apply 28VDC to Phase B wrt Phase C to hold motor at that pole. Wait ~1 second, then read the motor position via resolver.
- Apply 28VDC to Phase C wrt Phase A to hold motor at that pole. Wait ~1 second, then read the motor position via resolver.
Can this be accomplished with the DRV8312 kit?
Thanks,
Tim