Hello,
I'm migrating a TMS320C2810 project over, from CCS 3.1 to CCS V5.1. I can build the project, etc. Now I need to be able to flash the resulting output to the processor, i.e. the same thing done with F28xx On-chip Flash Progammer Tool in CCS 3.1. However, in CCS 5.1, as soon as I select Tools On-Chip Flash, it brings up the On-Chip Flash window, but has the message:
"Property for node name FlashProgrammerNode could not be found".
and nothing else. Can't do much flash programming, with that.
Please advise.
Robert
P.S. I'm using CCS 5.1 for other, separate projects (C6748) and Target Configurations, if that factors into this issue at all.