This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

linking problem building the control subsystem project from the F28M35x Firmware Development Package User's Guide

Other Parts Discussed in Thread: CONTROLSUITE

When I go through the "Getting Started and Troubleshooting"  Control Subsystem Project Creation procedure, and then build the project, (using CCS v5.2.1) I get:

**** Build of configuration Debug for project DC2020_C28 ****

C:\ti\ccsv5\utils\bin\gmake -k all

'Building file: ../main.c'

'Invoking: C2000 Compiler'

"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --vcu_support=vcu0 -g --include_path="C:/ti/ccsv5/tools/compiler/c2000_6.1.0/include" --include_path="C:/ti/controlSUITE/device_support/f28m35x/v_last/F28M35x_common/include" --include_path="C:/ti/controlSUITE/device_support/f28m35x/v_last/F28M35x_headers/include" --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"

'Finished building: ../main.c'

' '

'Building target: DC2020_C28.out'

'Invoking: C2000 Linker'

"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --vcu_support=vcu0 -g --diag_warning=225 --display_error_number --diag_wrap=off -z --stack_size=0x300 -m"DC2020_C28.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/include" --reread_libs --display_error_number --diag_wrap=off --entry_point=code_start --rom_model -o "DC2020_C28.out"  "./main.obj" -l"libc.a" -l"C:\ti\controlSUITE\device_support\f28m35x\v_last\F28M35x_common\source\F28M35x_CodeStartBranch.asm" -l"C:\ti\controlSUITE\device_support\f28m35x\v_last\F28M35x_common\source\F28M35x_usDelay.asm" -l"C:\ti\controlSUITE\device_support\f28m35x\v_last\F28M35x_common\cmd\28M35H52C1_RAM_lnk_c28.cmd" -l"C:\ti\controlSUITE\device_support\f28m35x\v_last\F28M35x_headers\source\F28M35x_GlobalVariableDefs.c" -l"C:\ti\controlSUITE\device_support\f28m35x\v_last\F28M35x_headers\cmd\F28M35x_Headers_nonBIOS.cmd" "../F28M35x_generic_wshared_C28_RAM.cmd"

<Linking>

".\ccsObjs.opt", line 1: fatal error #6001: cannot open file "./main.obj":  No

>> Compilation failure

   error

gmake: *** [DC2020_C28.out] Error 1

gmake: Target `all' not remade because of errors.

**** Build Finished ****

 

But main.obj is clearly observable in my Debug directory.  What have I messed up or forgotten?

Thanks for your help!

Larry