Other Parts Discussed in Thread: TMS320F2812
CCS 3.3.38
Emulator: TDS510USB 2.0
Target: TMS320F2812
Hi!
I am struggling in the following phenomena: 1000 NOP instructions need about 50 us with a clock of CLKIN or SYSCLKOUT of 150 MHz. I expected about 6ns per NOP what makes 6us for 1000.
Why is my processor working 8 times slower...?
These checks are already done:
- Measured the clock frequency at crystal with an oscilloscope.
- Verified if the PLL was initialized and if it works correctly
- Triggered my oscilloscope before and after running the NOPs to verify the speed of my CPUTIMER0 us-timer, used for performance measurements.
Any ideas?
thanks in advance. Timon Meier