Hi,
I am currently using the Motor Control and PFC Control Developers Kit kit to achieve speed and position control. I wish to use the F2808 control card with the above kit which is supplied with a F28035 control card. I wish to use the Ecaps on F2808 control card for position sensing. I am trying to figure out what changes I need to make to the examples supplied with the kit to enable the ecaps on the 2808.
I am wondering if I need to make any changes to the 2xPM_Motors-DevInit_F2803x.c
Also is there a source file for Initializing the Motor Control Dev Kit for use with the F2808 control card.
-Manas