This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ECAN controller: implementing an Rx FIFO

Folks, I originally inquired on this to the fine folks at TI who, as is so appallingly typical, immediately shrugged their shoulders and suggested that I come here and spend y'alls' time and effort instead....

So, without further ado, below is the bulk of my inquiry email to them; any takers here?

Thanks in advance.

 

When using a higher level protocol stack above CANbus, the desired model from a receive perspective runs more towards a FIFO rather than an array of discrete mailboxes, as one will tend to want to get a potentially arbitrarily large assortment of message ID that effectively render the acceptance mask facilities useless; one instead must run with ‘wide open’ filters, and do the filtering in software. From this view, the eCAN construction is quite atrocious, as, basically, a message received into a mailbox can be overwritten at any time, e.g. while it is being read out of the box. The only way to prevent this is to create a pseudo FIFO of some number N of mailboxes via the overwrite protection mechanism, where N corresponds to things such as the CAN bus’s packet burst size and other traffic characteristics for a given application, and  the device driver’s worst case interrupt latency and degree of preemption by higher priority ISRs, again for a given application, such that one can warrant the absence of overruns i.e. lost Rx messages.

So, one could e.g. create this pseudo FIFO using the range of mailboxes extending from #31 through #(31 – N + 1). And this range might well be the entirety of Rx mailboxes employed by the device driver.

However, the nature of the controller whereby, upon reception of a packet, it always begins its search for a mailbox (in which to place the message) with #31 and proceeds ‘downwards’ is problematic. Considering the ISR that services Rx’d messages: if there is a burst of Rx activity that results in storage in e.g. boxes 31-28 by the time that the ISR actually gets to where it can remove #31, how does it return that box to the controller? It can’t do it immediately, as e.g. a new or ongoing burst might then store into 31 & 27-25, and the temporal ordering of received messages is then lost, which can result in the failure of higher level protocols that presume (quite reasonably, in my view) that such ordering is preserved. So, in fact, this pseudo FIFO must have a length of 2N, with the ISR proceeding as follows:

- Start pulling messages at #31 and proceed downwards until either one runs out of messages or pulls N messages; don’t return the boxes to the controller

·         - For the case where the number of pulled messages is < N, resume pulling at the stopping point in one or more future ISR invocations until N have been pulled.

·         - When N have been pulled, return them all to the controller en masse, indeed, atomically. This creates a sufficient degree of ‘headroom’ so as to preserve ordering in the event of an imminent burst.

·         - In the same ISR invocation wherein N have been pulled, continue downwards until no more messages are found; if none are found then check again on the next ISR invocation, to address a possible race condition. Here, the 2nd half of the pseudo FIFO is being used to cover bursting, or traffic generally, that may have occurred during the aforementioned ISR invocations where the headroom consisting of the 1st half of the pseudo FIFO was being reacquired. Mailboxes in the 2nd half, as they are emptied, can be returned to the controller individually / singly.

·         - When it is certain that the 2nd half has been emptied, the process resumes with the 1st half.

So, all well and good, but how to negate the mailbox interrupt flag for boxes that have been emptied but are not ready for return to the controller? Sadly, it seems that both purposes rely upon the same action, i.e. the negation of a given box’s CANRMP bit!

And thus the actual question: how indeed to do this? Can I clear the given box’s CANME bit, and cause the negation, and later reenable it immediately prior to or after clearing CANRMP when I am ready to return it?  Would clearing CANME, and then CANRMP, do the job, with re-setting of CANME to effect the return? Are rubber chickens necessary?

 

  • Delsen,

    To preserve the temporal order of the received (or transmitted) messages, a time-stamp counter is available in the eCAN module. Have you explored that option? Each mailbox has a time-stamp register that preserves time of successful reception (or transmission)

  • HareeshJ,

    I have not, as it is, like much of the controller, not all that well documented, and my previous inquiries thereupon to TI were regarded as incomprehensible. And, I can't say as I'm particularly thrilled at the prospect of doing a sort at that level. But, thanks for the reminder; I'll take a look at that once I get a couple other problems beaten down.

     

  • Delsen,

    Please take a look at the example code titled MOTO.C from the app.note SPRA876B that you can download from the TI website. It is a very simple code that illustrates the timeout feature (and hence the timestamping feature). It is not exactly what you want, but gives you a feel for how to use the timestamping feature.

  • Hi folks,

    I finally got my CAN driver fairly well beaten into compliance, and wanted to share my results. First, though, let's review: I inquired about a specific area, both here and directly to TI support via email, and never got a reply. Instead, I, here, get something to the effect of "rather than directly respond to the issue, I'll suggest that you just make your driver more complicated by introducing a facility that you otherwise have no use for, and which requires that you spend yet more clock cycles - on sorting packets"; and, from TI support, I get: "well, since someone on the E2E has given you some kind of response, no matter how weak, we're not going to pursue the matter any further".

    Wow! Now that's Quality support!!

    NOT!!!

    Anyhow, left to my own devices (no pun intended), I eventually came across, in the plethora of controller registers, one by the name of CANMIM, i.e. CAN Mailbox Interrupt Mask; it's one of those where each bit relates to one of the 32 mailboxes. Of course, that name is a complete misnomer, as setting a bit, rather than masking interrupts for a given mailbox, actually enables them.... But, anyhow, if you want to defer returning an Rx mailbox to the controller, just set the corresponding bit to 0, and you've effectively cleared the interrupt that was generated for whatever event occurred on that mailbox; later, when you do want to return it, set the bit back to 1, and also do whatever you would have done had you not needed to defer the action, e.g., for a typical 'message received' event, write a 1 to the corresponding bit of CANRMP.

    If you're content with a single Tx mailbox, you can then, using the scheme that I previously roughed out, set aside 30 boxes for Rx, which enables you to tolerate situations where up to 15 worst case (i.e., short - 11 bit ID and no payload) packets arrive per each complete servicing via ISR.