Hi.
I am able to flash the .out file for the Periph-Runall.pjt project I have compiled without any problems. I can debug as well. Also, I can use the GUI program to connect serially and download the .a00 program file to the MCU. What I would like to do and am having trouble with is to debug the MCU with Code Composer while I'm using the GUI Program. If I try connecting the debugger (XDS510LC USB) while I am currently connected with the GUI program, the GUI program ceases to communicate. Is there a way that I can accomplish this?
Thanks,
Omer Peleg