This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can ADC external reference be 4.096 V?

I am looking at available external ref. for ADC for F28035 Piccolo. Recommended max. voltage for external ref. (VDDA) is 3.63 V. Can I use 4.096 V ref. since the absolute max on any pin is allowed upto 4.6 V ? How are recommended values derived ?

  • Please note the foot note which comes with absolute maximum ratings "Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability." It is better not to subject any pin with absolute max values. I personally try to saty with nominal values.