Hey,
I developed a hard and software based on the HVMotorCtrl+PfcKit to control BLDC Motors with the F28035 microcontroller.
Due to the need of a second QEP encoder we changed the hardware to the F28069 controller.
To adapt the software to the new hardware I changed all the used header files, the linker command files, ... as described in the sprabj2 TMS320F2802x/TMS320F2803x to TMS320F2806x Migration Overview. Additionally I changed the BLDC Sensored DevInit, f2803xbldcpwm, f2803xhall_gpio, f2803xileg_vdc and f2803xpwmdac files to the f2806x ones found in the BLDC_Sensored Project of the DRV8312-C2-KIT_v128 found in the Control Suite software.
After fixing several compilation failures caused by the change of the header and driver files the project could be build without any errors. Although the RS-485 communikation and the SPI communikation with the new prozessor works fine.
But when i connect a Motor to the new hardware it don´t react as expected. It seems that there is a problem in the control of the Motor with the added files.
Did someone get similar problems by migrating from 2803x to 2f806x?
Did i forget anything important by converting the project from f28035 to f28069?
Is it principle possible to use the F28069 with the same _IQ math as the fixed point f28035?
Thank you very much for your time
Regards
Joachim