This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335/332 flashing troubles

 Hallo, im using three  28335 and two 28332. I downloaded last update for ccs from site and tryed to flash mcu. i can flash 28335 but i cannt flash 28332, ccs said me what "part id is oxffff try to look at 0x380090". i looked up there and really 28332 contains 0xffff there! but 28335 contains its own part id. i use examples from site, folder "flash" - just opening the project (35 or 32), compile and try to flash. also a tryed to change gel file but it did not help. i think the ccs is searching for part id in wrong place on 332, but i cannt understand how to solve it :/. i'm using sau 510 plus usb emulator, ccs with last updates. program works well in ram.