Other Parts Discussed in Thread: TMS320F28023
I'm starting a new project to drive 2 half-bridges, measure 2 currents and 2 temperatures.
In case of overcurrent, I'd like to stop ePWM outputs inmediately, without ADC. TMS320F28023 has 2 comparators which share pins with ADC inputs. Is the comparator able to stop ePWM while the ADC is measuring the same pin?, is it able to do it asynchronously?, do I have to use 2 different pins for the same signal (one for comparator and another one for ADC)?, or do I need external comparators with outputs connected to TZx (trip-zone) inputs?.
Thank you in advance