I am using 2810 micrcrocontroller for STATCOM application(Three level inverter).
In the starting all PWMs from EVA and EVB should be pulled low.(ACTRA &&ACTRB=0x0000).
Ones the initial check is done for the healthyness of the inverter one digitalinput will be high.Once the dsp gets this signal it makes (ACTRA &&ACTRB=0x0666).
But the same I am unable to do .
The PWM output becomes :=>
PWM1 to PWM6 = all high(EVA)
PWM6 to PWM12=all low(EVB)
KIndly help....
Prashant