Hello TI,
I took advantage of the MCU Day discount and picked up one of the TMDXDOCK28346-168 kits - but it appears that the 28345 Control Card was shipped vs. the 28346.
I have CCS v4 installed under Vista-32 and Vista-64 - but unfortunately I can't get the debugger to start on either. Eclipse prints out an error dialog with JVM terminated. Exit code=1.
The DSP on the control card has some 'crud' on it - so it is hard to tell if the 5th digit is really a 5 or 6 - I was hoping to get the debugger up so I could tell for sure.
Thanks In Advance,
johnw