Hi,
I count a float / int variable up to 100 and logg the data, is the value 100 i set it back to 0.
in the sawtoth i have steps and the ramp works after the step normaly but i don´t can find a reason for the steps.
I write the value to the epwm show the value withe the oszi and the steps are not a displayproblem withe the time/frequency graph it is a real step in the value...
The steps are in the variables in my epwm and in independent variables in the idle loop mostly at the same time.
Thanks for help.
Chris