This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a question on the DMA Access on the TMS320F28335. I want to confirm that If I have the DMA writing to one of the memory interfaces, the CPU can access all the other interfaces at the same time, the only time there would be a conflict is if you try and access the same memory interface from both the CPU and the DMA. For example if I use the L7 RAM for DMA acceess, the L4, L5 and L6 RAM as well as the external RAM can be accessed by the CPU without risk of confilct.
Can someone please confirm that this is correct?
Thanks
Ed
Hi Ed,
Yes, CPU and DMA can access different RAMs at same time without conflict. So DMA can access L7 and same time CPU can access other RAMs without any issue.
Regards,
Vivek Singh