This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS510PP plus emulator

Hi,

I am using a XDS510PP plus emulator to connect to a TMS320F28335SPGFA. I had no problems in communicating with the target initially. Few days back, the emulator stopped connecting with the target. It gives out a error telling Fatal Error during OCS. When i run the diagnostics using the SDconfig tool, it passes the JTAG test indicating that the JTAG connectivity is fine.

I tried to use the same JTAG emulator with other boards having other DSP's and found that there are no issues. I have another XDS510PP plus emulator with which i tried connecting the boards having TMS320F28335SPGFA and this emulator connects to all these boards.

When i run the Code composer setup or the SD config tool, i dont see the XDS510PP plus options. All the options are for XDS510PP and not for XDS510PP  plus. Has it got to do something with the drivers?

The problem now i face is that the first JTAG emulator doesnt connect to any of the DSP boards with TMS320F28335SPGFA controller. Have anybody come across this issue?