Hi All -
I hope that posting this question to the C2000 area will be relevant to the group.
I have just successfully installed CCS4 and converted an existing CCS3.3 project. I can run the code generation tools and the debugger but I am missing one of my favorite debug tools. In CCS3.3 under the GEL menu I usually see scripts to add peripheral block registers to the watch window; for example Watch ADC Registers, Watch ePWM Registers, etc. Are similar scripts available for CCSv4 for the C2000 targets? If so, can someone point me to the appropriate setup documentation? I am using a x2806 target board.
Thanks in advance,
Gary