Is there any manual for moedling v/hz open/closed loop control of 3ph induction motor using embedded target for TI C2000 - f2812 ezdsp? please HELP me....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any manual for moedling v/hz open/closed loop control of 3ph induction motor using embedded target for TI C2000 - f2812 ezdsp? please HELP me....
In Matlab/simulink R2009b you will find a Demo Called "Simulation of FOC Using PMSM Model" but you will need SimpowerSystems Toolbox and an Spectrum Digital F2812 eZdsp to use this.
There is also a step by step Tutorial under the Demo "Motor Control" .
Hope this will help you.
No wonder. I'm currently using the R2006a version. Thank you so much for replying. Do reply again if you have any info regarding constant V/hz control. Actually my project requires me to get familiarize with the eZdsp f2812 by implementing the mentioned speed control of 3ph ACI motor. Thanks again.
Hello - Initially you may consider using example projects to get yourself familiar with the controller and the algoritm. These example projects are available from TI websites and I believe there is one CCS project implementing 3 Phase induction motor drive with V/Hz algorithm.
Yes, in the meantime you can evaluate F281x ACI 3PH V/Hz control using
http://focus.ti.com/docs/toolsw/folders/print/sprc130.html