This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320f240pqa instead of -pqs

Hi

tms320f240PQS is well used ongoing MP now for Inverter control board.

but this device has occured a delivery issue,

so changed to tms320f240pqa instead of tms320f240pqs.

after that, board of tms320f240pqa is not work at all.

As I know these two deice is 100% direct  pin to pin compatible,

the only different is the temperatuer Spec.

Is that reight?

If you have an experience or tip, please let me know..

Thanks,

eric.