Hello,
I have a few questions regarding the ADC module on the TMS320f2808, specifically with the ADC input channel select registers. Is it possible to safely change the values of the channel select registers while and ADC sequence is running, such as in continuous run mode? When exactly do the channel select registers get accessed by the ADC and is there any arbitration logic to prevent these registers from becoming corrupted if they are written to when the ADC reads them? I am having trouble finding a clear answer to this in the documentation.
Thanks