I've got C code running on a 2808 board that works fine when built with 4.1.3 tools. Since I've upgraded to 5.2.2, it appears a bug has developed related to the SP getting trashed in an ISR. I can re-build with 4.1.3 and the SAME exact code works fine.I can go back and forth between build versions, and the 5.2.2. consistently fails.
Ti, please respond to this as I've seen another thread related to bugs in 5.2.2. I don't have any other versions installed between 4.1.3 and 5.2.2, so I don't know at which build it was introduced.