This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem to flash the F28035 with external oscillator set



Hello,

I'm actually working on the experimenter kit Piccolo B (F28035) and try to work with the external oscillator (I added the oscillator X1 and the resistor R4). This is working fine using the RAM but it is not possible
for me to flash the device. The Clock Configuration field are "shaded" and it is not possible to change the default value (OSCCLK 10MHz, DIVSEL /2, PLLCR 2). My external oscillator is 20MHz and I set 3 for PLLCR
and 2 for DIVSEL.

- CSS: 3.3.82.13
- Code Generation Tools: 5.2.2
- I as well installed the plugin allowing to use the F28035

Does someone havi any idea why I'm limited for this configuration?

Thanks,
Steve