Other Parts Discussed in Thread: TMS320F28065, TMS320F28035, CONTROLSUITE
Hi all,
I have some questions regarding Piccolo 28035 CLA:
1) If I understand the datasheet right, CLA code can only be run from L3 (CLA program RAM). It can be loaded from flash and run in L3
2) There is no different CLA prog region other than L3.
3) I can configure L3 to be accessible by the CPU (MEMCFG.PROGE=0) or by CLA (MEMCFG.PROGE=1).
It can't be accessed by both the CPU and the CLA.
I have to switch the complete L3 RAM (4k) to CPU or CLA.
The same appears for CLA data RAM in L1 and L2.
Are these assumptions correct?
If yes, then this limits the usage of the CLA: I have to spend 4k of the limited 10k Piccolo RAM for CLA program space even if I only use 50 words of it!
I hope there is still some misunderstanding on my side...