This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

effort in unlocking CSM via brute force method

I am evaluating the security features and want to find how hard is it to unlock CSM via a brute force method.  Assuming a good random key was programmed into the CSM and have a dedicated hardware setup to run JTAG and try brute forcing all combinations.

I believe there nothing in the CS that prevent brute force approach ( like time out after few tries etc.).  In this case, programming with all zeros and permanently locking CSM should prevent brute force method. 

Thanks,

Sandeep