When DSP 28035 is used as master to communicate with other devices through SPI, I should use SPISTE (GPIO27, GPIO15 or GPIO19) to enbale slave transmit (assuming active low here). Could I use other general purpose I/O except for the three mentioned above to enable the slave transmit? If that doesn't work, how can I enable three SPI communications (three devices) through three transmit enable pins asynchronously?