Hi all,
the piccolo boot rom documentation sprufn6.pdf and sprugo0.pdf tells that part of M0 (0x0002 to 0x004E) is used during boot-load process and no code or data should be bootloaded into this address range.
The examples mark this region as "reserved", too.
I would not like to waste ram and use this in application code, for variables or application stack. I think this should be okay since application code runs after the boot-load process.
Is this correct? Can I use the boot rom stack reserved memory for application memory after the boot-load process?