it writes,
This API can plug the full set of vectors supported by the PIE (0-127). If
the PIE is not enabled, the vector will be plugged in the default vector
area. If the PIE is enabled, the vector will be plugged in the PIE vector
area.
If the default vector is set in the internal rom, from the address 0x3FFFC2 to 0x3FFFFF, what will happen?