This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Prime development package update

Other Parts Discussed in Thread: AFE031

Where can I download an updated dev. package? I'm using the software that came with the TMDSPLCKIT-V3, but looks like something is missing because the example code doesn't compile, at least with my setup:

1.- Installed the latest CCS for Linux from TI site in my Linux  (Ubuntu) system.

2.- Installed the prime dev. package that comes with the pendrive into a Windows partition,

3.- Copied everything under FW (in the windows partition) to my Linux system

Then I created a new Workspace (by importing the project with Project -> Import Existing CCS Eclipse Project), but the compiler complains and stops:

**** Build of configuration Release_F2806x_AFE031 for project test_tx_rx ****
/opt/ti/ccsv5/utils/bin/gmake -k all
subdir_rules.mk:6: ** target pattern contains no `%'.
Stop.
**** Build Finished ****

Does anybody got a similar error or could guide me on how to compile the test_tx_rx example?

Thanks!

Carlos