Other Parts Discussed in Thread: TMS320F2808
Hi,
I'm having trouble using the RFFT_f32_sincostable routine in C28x_FPU_lib. I'm compiling it with the following options:
[RFFT_f32_sincostable_IQ.c] "C:\Program Files\C2000 Code Generation Tools 5.0.1\bin\cl2000" -g -pdsw225 -o3 -fr"C:/tidcs/c28/C28x_FPU_Lib/beta1/source/Debug" -i"../include" -d"alignbuf" -d"_DEBUG" -d"LARGE_MODEL" -ml -v28 --float_support=fpu32 -@"Debug.lkf" "RFFT_f32_sincostable_IQ.c"
When I run it in the simulator, I see the following assembly:
3E81A3 RFFT_f32_sincostable:
3E81A3 B2BD MOVL *SP++,XAR1
3E81A4 AABD MOVL *SP++,XAR2
3E81A5 A2BD MOVL *SP++,XAR3
3E81A6 E203 .word 0xE203
3E81A7 04BD SUB ACC,*SP++ << 16
3E81A8 E203 .word 0xE203
3E81A9 05BD ADD ACC,*SP++ << 16
3E81AA E203 .word 0xE203
3E81AB 06BD MOVL ACC,*SP++
3E81AC FE02 ADDB SP,#2
3E81AD 82A4 MOVL XAR3,@XAR4
The simulator hangs at the 4th instruction down: ".word 0xE203".
Any ideas what I could be doing wrong? ".word 0xE203" doesn't appear to be a valid assembly instruction.
Thanks,
Eric