Other Parts Discussed in Thread: CCSTUDIO
Hello,
I have some difficulties connecting to my F28335 eZdsp board. I tried connecting using the on-board JTAG emulator and external XDS510 USB and XDS510PP Plus emulators, and faced error messages in all three cases. After uninstall/install of the "eZdsp28335 Drivers and Target Content" package (with antivirus disabled), I managed to connect using on-board emulator. But after a while, this stopped working and now again I can't connect... CCS reinstall doesn’t help either.
If I try to connect using on-board emulator or XDS510USB, CCS responds with error message:
---
Error connecting to the target: Error 0x80000200/-1135 Fatal Error during: OCS, Unrecoverable emulation error
---
With XDS510PP PLUS, CCS displays:
---
Error connecting to the target: Error 0x80000200/-1145 Fatal Error during: OCS, Unrecoverable emulation error Sequence ID: 0 Error Code: -1145 Error Class: 0x80000200
---
I tried testing external emulators using SdConfig v3.3, and got following results:
- for XDS510USB:
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
ERROR >> JTAG IR scan test failed
>> Check power to your emulator/eZdsp
>> Then check your port mode/address
- for XDS510PP PLUS
** Emulator Test **
$$ EmuProductName=XDS510PP_PLUS
$$ EmuPortAddr=0x378
$$ EmuPortMode=SPP8
$$ ProductId=10
$$ ProductVersion=02
** Emulator Scan Test
ERROR >> JTAG IR scan test failed
>> Check power to your emulator/eZdsp
>> Then check your port mode/address
These two emulators are working properly with other EVM, eZdsp and custom boards based on F240, F2407 and F2812 controllers.
I scoped XCLKIN (at U11:3) and XCLKOUT (at P2:48) signals and power up sequence (PONRSnIN, VDD and VDDIO – at U9:28, U9:23 and U9:18) on the eZdspF28335, and they all seem OK.
Here is what I am using:
- CCS
* ver 3.3.81.13
* IDE 5.98.0.393
* BIOS 5.31.02
* cgt v4.1.3
- eZdspF28335
* S/N C2E_0805178
* rev B
- XDS510USB
* serial 2005/09-244
* rev B
- XDS510PP PLUS
* serial 2005/08-018
* rev A