This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 motor control library based on 2812 and 2808 code

Hello,

I am working on a project that consists of porting motor control code designed for the 2812 DSC to use in the F28335 DSC. I have been working with sample code from the 2808/2809 family in order to adapt the EV modules into ePWM code, but I'm getting somewhat lost during the conversion process.

I have been referencing the SPRAAQ7A document on Migrating from the 281x to 2833x, as well as the SPRU065E document on the Event Manager and the SPRUG04 document on the 2833x ePWM module, but this is becoming a drawn out process.

I was wondering if there were other recommended documents to look at to help with the conversion process, or if there is possibly some sample code available to assist with the conversion process?

Thanks for the help!