Hi,
Target : TMS320F2812
Emulator : SPI515 Parallel Port
IDE : Code Composer Studio v3.3, Evaluation
Code Runs in : Flash Memory
Problem:
Is there any wayout to debug a target which was flashed with 128-bit Code Security Module Password(known) without reflashing the target with all 128-bit CSM Password fields with '1'(eight no.s of 0xFFFF), if we know the password?
That is, has there a way to tell the emulator that 'this is the password' and let him debug without reflashing the 128-bit CSM fields to '1'?
Sincere thanks for any help!
---------------
-Regards, Sinoj