Other Parts Discussed in Thread: TMS320F28335
hello
i am working with the TMS320F28335 MCU and have worked out how to use the hex2000 tool and the flash api. however i am unsure as to which options i should use for the hex2000 tool to be able to put the hex output into a buffer in my code and then program it to flash as an application. i want to be able to jump straight to the memory where it was programmed and for the application to start running from there. this is for a bootloader project.
thanks
michael