Other Parts Discussed in Thread: DRV8312, INSTASPIN-BLDC, CONTROLSUITE
E2E forum information, per the guidelines:
Host OS: Windows 7 Home Premium, Service Pack 1
CCS Version: 5.2.1.00018
DRV8312EVM 6517813 Rev D
CC2803x ISO DIMM REV 1.3
Texas Instruments XDS100V1 USB Emulator
Awhile back I posted regarding the use of the DRV8312 kit w/ InstaSPIN-BLDC on my motor. After making the recommended changes from the link below, it has run ok up to about 24,000 rpm. I've learned that this motor produces a sinusoidal BEMF, which makes me think the motor would run more efficiently with FOC (using the PMSM Sensorless project). I'm having some of the same problems I encountered before. I have a few questions:
1) Should I expect that the PMSM Sensorless project (from controlSUITE) can be used with the DRV8312 kit to drive my motor at 30,000 RPM? I don't want to spend a lot of time fighting this if this is beyond the hardware limits of the equipment. I'm using an 18V bench power supply to power the board, and my motor only draws about 500mA (fully loaded) at 22,000 RPM using the InstaSPIN project.
2) The advice from the previous post was to change out the caps on the current sensing circuitry to smaller values (10nF). I've tried using DRV8312 kits both with the original caps and new caps, but the new caps don't seem to help. However, I'll keep trying if there's no reason to expect the original caps to work at 30,000 rpm.
Any assistance is appreciated. Thanks.
Previous post: