Hai All
I am new to this community and F28335 controllers.
I am working with F28335 using CCS Ver3.3,Signums JtagJet Emulator(USB2.0).
I am trying to load the example code to the target,at that time it is giving the following errors.
1. Data verification failed at address 0x8000
Please verify target memory and memory map.File laod failed
2. Invalid comiler option __float_support = fpu32
3. Entry point other than _C_int00 specified
How to fix these problems.I never faced these type of problems on F2812.
What may be the wrong for above errors.
Thanks
Srinivas reddy