This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't start Piccolo Experimenter's Kit CCS?

I'm trying to use the Limited version of CCS that came with the F28035 Experimenter's Kit,

and I can't even start the program.

 

If I start up CCS (via the icon) it runs cc_setup -- Vista has to ask my permission to do it --

and then reports "Error Reading Code Composer Setup information/Code Composer may

not have been correctly installed".

 

If I start CC Setup (via the icon), then "Save and Quit" I get "Code Composer Application

has stopped working". (The Vista Event Log says simply "crashed".)

 

I have (re-)installed CCS multiple times, using "Typical Install" and all the default settings. I

even installed ActivePerl, though I thought it wasn't required just to start the program.

I can see cc_app.ini and cc_setup.ini in cc\bin, and there's nothing obviously weird

in them. (I checked the shortcuts and they do "start in:" cc\bin.)

 

Searching the Forum, no one else seems to be encountering this. Am I missing

something?