Other Parts Discussed in Thread: TMDSDOCK28335
By Chintan Chauhan in TMS320C2000 Microcontrollers
Hi to all,
I am working on Experimenter's kit TMDSDOCK28335, that docking board has on board usb emulator XDS100 USB emulator. This experimenter's kit include Docking board with USB emulator on it, F28335 card, USB cable and CCSv3.0 32K byte limited size comiler.
I have installed that CCSv3.0 and than i had connected onboard emulator along with F28335 card inserted in the slot so when i cojnect it via USB supply it detected as a new hardware found named Dual RS232 and i m not able to provide driver to this card...
AS I have seen in the video demonstratio they are saying as i install CD driver will get automatically installed and on connecting that with the help of USB it will show "XDS100 Ch"1 or something like that with the symbol of USB and it will get installed.
But in my case it is not showing USB symbol on attachment .
I had checked this thing on other computer also but the problem is same.
Any one has faced this problem...???
Regards,
Chintan, R&D Engineer, [TRINITY, BARODA]