Other Parts Discussed in Thread: SPRC074, TMS320LF2407A
Hi,
We have a customer who is using TMS320LF2407A in their design. In their application they cannot use JTAG (due to long distance between end-equipment and Computer) to program the controller - so they are using serial utility(sprc074). But this serial utility works with Windows 98 only, while new version of CCS works with winXP. Is there any serial utility which can be used for programming with winxp or higher version?
They looked at codeskin c2000 programmmer but the problem is that it support LF2407A with external clock freq of 10 MHz or 20MHz, while they have external clock of 8MHz.
Pls suggest if there is any tool/ utility or work around to solve this problem.
Thanks,
Hitesh