This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB cable?????

I have a problem with the target ezdsp28335 (see error connecting dsp and error connecting target) i tried re-installing the driver for the emulator, re-installing the code composer, reset the emulator, but nothing works.

I change the USB cable and for my surprise the ezdsp28335 start to work fine, so i run a program and it work. But this was for a little time because next when i use a program that use RTDX the emulator error came up. 

So my next question are:

1) The processor work and the target still work fine, the emulator run just for a little, then what could be the big problem?

2) If i use an external emulator, there is a chance to eliminate this problem?

3) If the external emulator is the answer for my problem, i need other program to run the ezdsp?

4) What kind of emulator will i have to use?

Gaston