This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F38335 GPIO's timings

Hi folks!
 
I am working on an application which uses TMS320F38335 GPIO pins. In order to watch the GPIO timings performance, I have made the DSP to perform an infinite loop in which an single GPIO pin is put high and inmediately  put low. I have tested the timings and I have noticed that the time between a the rising edge of the level on the pin and the falling edge is around 50 ns. I believe it should be faster. The DSP PLL is set at 150MHz. Does anybody  know why this cannot meet the expected performance?
 
Thank you in advance