Other Parts Discussed in Thread: CCSTUDIO
I would like to see the signals in the CC graphs which I set up exactly like described in the documentation of this particular module. Unfortunately the signals I see are completely strange and have nothing to do with the signal I should see. Strangely the real PWM Output signals of the controller are looking OK on the oscilloscope. So my conclusion is that the Signals, which comes out of the SVGEN_DQ module are also OK. But why is the graph so strange?. I tried to watch other modules with the CC graphs like the Output of the RAMP_GEN module. I should see a ramp function. But this signals are also completely strange. Can anybody help me here since nobody in this lab worked with CCstudio before and I am a student working for the first time with it. Thanks for your help. Maybe I can post the code to an email address?