This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I need a skeleton 28015 project for CCS3.3

I have the latest patch for CCS3.3 The CCS3.3 tconf.exe creates a platform OK, but there is no 28015 in the list of supported DSPs.   So I used the 2801 for the user editable file to create my  platform.  I need the tcf file because I am using legacy 2812 code which uses realtime features of DSP/BIOS.  When I select New>DSP/BIOS Configuration and select my platform there are errors in the Javascript boilerplate which I have not edited(and is protected against editing).  It appears that CCS3.3 has some broken script links so I cannot create the config  file for the project.  Does anyone have a skeleton 28015 project with a .tcf file and cmd files I can use to jumpstart the project?

This question is also posted on the general Digital Signal Processor forum.