This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 Power Line Modem Developer's Kit issue

Hello,

 I'm Vinícius Fonsêa Nobrega, I am a Master's student of UFCG's Electrical Engineering course. The C2000 Power Line Modem Developer's Kit can be of great help in my research, but before acquire this kit I need some questions answered. 
1st. The white paper IT Delivers Flexible Power Line Communications Solutions interested me when I read: "IT is supporting a proprietary, fully-programmable OFDM-based system with the FlexOFDM™ library, Which Allows developers to further Top Improve efficiency by tuning performance and robustness for specific environmental factors or , if required, quickly sets the custom OFDM Implementation with configurable frequency band, number of data tones, etc.. ", but I have not found in its API (The PLC GUI Class Library in sprcad0's software) functionalities that proves this feature. I found some tools, such as FleLiteBand and ToneMapRequestMode, but nothing specific. I would like to confirm that it is actually possible and which functionalities confirm that. 
2nd. Is possible to create a communication scheme that uses MAC and PHY layer of PRIME with FlexOFDM perform little changes in OFDM technic, in data tones, for example ? 
3rd. The kit includes a base code that supports the development? 
Hope fast reply, because I'm running out of time for this research. Best regards, 

Vinícius Fonsêca Nóbrega.