I am using TMS320F28335. My SYSCLK is 120MHz, and LSPCLK being 60MHz
I am trying to achieve higher speed on McBSP interface with DMA - upto 20 Mbps
I could get a maximum of 4Mbps only. Is there any special requirement to achieve higher speeds
On speeds higher than 4 Mbps, i donot get receive interrupt at the receiving end or at times get aroung 50% of the actual transmitted packets.
Any help Please.
- arpan