This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Delfino 300MHz = Happiness!



Hi:

I have been aching for more clock speed from C28x for a while now.  Thank you TI!  Oh, and the larger amounts of full-speed RAM are yummy too!  Can't wait to use up all the cycles on one of these babies...  Actually, using up cycles is rarely my problem.  I often do wierd stuff requiring the absolute fastest possible interrupt latency, but with only a small % of the CPU's total processing power being taxed.

How long before I'll be aching for even more clock speed after that :-D

This Delfino will hopefully keep me from considering ADI Blackfin for quite a while.