Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI DAC with the TMS320F2812

Other Parts Discussed in Thread: TMS320F2812

Hi,

I'm having some trouble trying to transmit from the SPI peripheral with my TMS320F2812.  In my configuration, the DSP is the master and the DAC is the slave.  The DAC is an LT2622 (12-bit), but my problems starts even before trying to successfully send commands to the DAC.  I'm not seeing the correct signals coming from the SPI lines themselves.

Here's how I'm configuring the peripheral:

void SetupSpi(void)
{

    EALLOW;                                    //Setup peripheral clock for SPI
    SysCtrlRegs.LOSPCP.all = 0x0002;
    SysCtrlRegs.PCLKCR.bit.SPIENCLK=1;
    EDIS;


    //SPI Configuration Control Register:
    SpiaRegs.SPICCR.bit.SPISWRESET = 0;        //initialize operating flags
    SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;    //Data output on rising edge
    SpiaRegs.SPICCR.bit.SPILBK = 0;            //disable loopback for now, testing...
    SpiaRegs.SPICCR.bit.SPICHAR = 0xF;        //setup for 16 bit words
       
   
    //SPI Operation Control Register       
    SpiaRegs.SPICTL.bit.OVERRUNINTENA = 0;    //Disable overrun interrupt
    SpiaRegs.SPICTL.bit.CLK_PHASE = 1;        //Data is output one half-cycle before the first rising edge of the SPICLK signal and on subsequent falling edges of the SPICLK signal; input data is latched on the rising edge of the SPICLK signal       
    SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;    //Configure SPI as master
    SpiaRegs.SPICTL.bit.TALK = 1;            //transmit enable pin enabled
    SpiaRegs.SPICTL.bit.SPIINTENA = 0;        //Disable SPI interrupt



    //SPI Baud Rate Register
    //SPI Boud Rate = (LSPCLK)/(SPIBRR+1), for SPIBRR =3:127
    SpiaRegs.SPIBRR = 63;    //~1.3MHz for now                   

    //SpiaRegs.SPIFFCT =                     //SPI FIFO Control Register
    //SpiaRegs.SPIPRI =                     //SPI Priority Control Register


    }

 

Here's my test loop, in which I'm trying to get the DAC to switch between two values:

// IDLE loop. Just sit and loop forever:
   for(;;){

        SpiaRegs.SPITXBUF = 0x3F;         //command
        SpiaRegs.SPITXBUF = 0x3E80;    //data 1000

        delay_loop();

        SpiaRegs.SPITXBUF = 0x3F;         //command
        SpiaRegs.SPITXBUF = 0xBB80;    //data 3000

        delay_loop();


   };

What I'm seeing is the SPICLKA and SPITEA lines are staying low and the SPISIMOA line is just toggling at the period of the delay in the loop.  I'm not seeing any data being sent from the peripheral. 

What am I missing here?  Any help is appreciated.  Thanks!

 

Jason